Verasys schedules - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
You can use the SBH to create and update system schedules. You can also use the SBH to synchronize different devices on the network for all connected devices and equipment. The Smart Equipment devices, including the TEC3000 Thermostats, and Verasys Application Controllers, contain embedded schedules that you can synchronize from the SBH. The SBH supports unlimited schedules in which you can assess and modify schedules hosted on remote devices. The maximum number of exception schedules allowed is 20.

The SBH supports the creation of local On/Off and Occupied/Unoccupied types of schedules. These schedules are associated with objects hosted in devices that do not support the feature locally. For example, devices such as the TUC and the ATC. See the following video link https://docs.jci.com/bas/verasys-schedules.