Plan the zone bus layout. For more information about communications buses, refer
to the Verasys BACnet MS/TP Communications Technical Bulletin
(LIT-12012362). If you use a wireless system with TMR100, refer to the Verasys
TMR Series Wireless Router Installation Guide (LIT-12014167). The steps below also
apply for a TMR wireless system. If you plan a TMR wireless system each device requires a TMR
to be connected with 22-3 awg shielded cable to the system bus or zone bus, instead of daisy
chain wiring to each device. The TMR100's form a wireless communication network that replaces
a hardwired network.
Note: Wireless NS8000 sensors can only be used with
WRZ7860 connected to the sensor bus of a controller. Refer to WRZ Series One-to-One
Wireless Room Sensing System Technical Bulletin (LIT-12011641)
It is best practice to connect the devices in the following sequence:
- Install the SBH200 in a location that is easy to access.
- Install the zone coordinator in a location that is easy to access, preferably close to the SBH200.
- Use 22-3 awg shielded cable to connect the blue four screw terminal system bus plug J12 of the zone coordinator to the same system bus plug on the SBH200 or other system bus device in a daisy chain configuration. Devices on the system should be addressed from 5-105, one-by-one, in sequence. The EOL switch must be set to the on position on the first and last devices on the system bus. All other devices must be set to off.
- Use 22-3 awg shielded cable to connect the gray or brown four screw terminal zone bus plug J11 on the zone coordinator to the RTU controller followed by the ZEC510 VAV box controllers in a daisy chain configuration. Devices on the zone bus of each zone coordinator must begin with address 5 and progress sequentially, one by one, up to 38. The EOL switch must be set to the on position on the first and last devices on the system bus. All other devices must be set to off.
Note: If you install two or more zone
coordinators, the devices on the zone bus of each indvidual zone coordinator must begin at
address 5. Duplicate addresses on seperate zone buses is permitted. For full wiring details
and diagrams refer to the Verasys ZEC310 Zone Damper and BYP200 Bypass
Damper Controllers Installation Guide Part No. 24-10143-1248 or ZEC510 VAV Controllers Installation Guide (Part No. 24-10143-01485).