Removing a profile from a BACnet device - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
About this task

Removing a profile from a device removes it from all Verasys features.

To remove a profile from a BACnet device, complete the following steps:

Procedure

  1. Click on the device in the device list and navigate to the Profile view.
  2. Click the Reset to defaults button at the bottom of the page to disassociate the profile from the device and rediscover the device inside of Verasys.