Data share - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
You can use the data share feature to share the value of a point from the list of shareable points from one device to other devices. The data selection defines what object or parameter is available for sharing to controllers with similar objects. The source selection sets which controller is the source. The destination selection sets the controller that receives the data.

Outdoor Air Temperature (OAT) is an example of data share. Instead of installing a physical sensor on every unit, you can connect a single OAT sensor and share the value to all other equipment. Occupied setpoints are another example. Set one device as the source and all other devices as the destination. You can simply change the setpoints on one device and share to all others.

Note: When you share the occupied cooling setpoint and unoccupied heating and cooling setpoints, the RTU becomes the master controller for the space. The fan coil unit setpoints match up to the master RTU. Verasys sends the source data values to the destination controllers when the value of the data changes. If a destination controller goes offline and then comes back online, the data share function sends the latest value to that controller. Refer to the following video link https://docs.jci.com/bas/verasys-setup-data-share.

To configure data share, complete the following steps:

  1. Click the Data Share tab.
  2. Click the Add Data Share button.
  3. In the Data drop-down list, select an object or parameter.
  4. In the Source drop-down list, select the controller that you want to define as the source.
  5. In the Destination drop-down list, select the controllers that you want to share the data with.

The following table lists the shareable data points.

Table 1. Shareable data points
Controllers Data in Data out
Smart Equipment Rooftop Unit, SE-SPU100xx-1 Humidity Setpoint Humidity Setpoint
Indoor Air Quality Indoor Air Quality
Occupied Cooling Setpoint Occupied Cooling Setpoint
Occupied Heating Setpoint Occupied Heating Setpoint
Outdoor Air Temperature Outdoor Air Humidity
Standby Cooling Setpoint Outdoor Air Temperature
Standby Heating Setpoint Standby Cooling Setpoint
Unoccupied Cooling Setpoint Standby Heating Setpoint
Unoccupied Heating Setpoint Unoccupied Cooling Setpoint
Zone/Space Temperature Unoccupied Heating Setpoint
Warm/Cool Adjust
Zone/Space Temperature
Discharge Air Temperature
Terminal Equipment Controller, SE-TEC3xxx-0 Common Setpoint Common Setpoint
Humidity Setpoint Humidity Setpoint
Occupied Cooling Setpoint Occupied Cooling Setpoint
Occupied Heating Setpoint Occupied Heating Setpoint
Outdoor Air Temperature Outdoor Air Temperature
Standby Cooling Setpoint Return Air Humidity
Standby Heating Setpoint Standby Cooling Setpoint
Unoccupied Cooling Setpoint Standby Heating Setpoint
Unoccupied Heating Setpoint Unoccupied Cooling Setpoint
Zone/Space Temperature Unoccupied Heating Setpoint
Warm/Cool Adjust
Zone/Space Temperature
Discharge Air Temperature
Verasys Generic IO Controller, LC-VAC1002-0 NONE Indoor Air Quality
Outdoor Air Humidity
Outdoor Air Temperature
Zone/Space Temperature
Discharge Air Temperature
Verasys Constant Volume Application, LC-VAC1000-0, LC-VAC3000-0 Discharge Air Temperature Discharge Air Temperature
Humidity Setpoint Humidity Setpoint
Outdoor Air Temperature Indoor Air Quality (CO2)
Standby Cooling Setpoint Outdoor Air Humidity
Standby Heating Setpoint Outdoor Air Temperature
Unoccupied Cooling Setpoint Standby Cooling Setpoint
Unoccupied Heating Setpoint Standby Heating Setpoint
Zone Temperature Setpoint Unoccupied Cooling Setpoint
Indoor Air Quality (CO2) Unoccupied Heating Setpoint
Zone Humidity Zone Temperature Setpoint
Occupied Cooling Setpoint Zone/Space Temperature
Occupied Heating Setpoint Zone Humidity
Zone Temperature
Third-party RTU controller, LC-VEC100-0 Outdoor Air Temperature Outdoor Air Temperature
Zone Temperature from ZEC Supply Air Temperature
Return Air Temperature
CO2
VAV Box Controller, LC-ZEC510-x, LC-ZEC310-0 Occupied Cooling Setpoint Indoor Air Quality
Occupied Heating Setpoint Occupied Cooling Setpoint
Standby Cooling Setpoint Occupied Heating Setpoint
Standby Heating Setpoint Standby Cooling Setpoint
Unoccupied Cooling Setpoint Standby Heating Setpoint
Unoccupied Heating Setpoint Unoccupied Cooling Setpoint
Warmer/Cooler Adjust Unoccupied Heating Setpoint
Zone Temperature Warmer/Cooler Adjust
Zone Temperature
Advanced Terminal Unit Controller, LC-ATC1xxx-0 Fan Mode Fan Mode
Heat Cool Mode Heat Cool Mode
Indoor Air Quality Indoor Air Quality
Outdoor Air Temperature Outdoor Air Temperature
Standby Cooling Setpoint Standby Cooling Setpoint
Standby Heating Setpoint Standby Heating Setpoint
Unit Enable Unit Enable
Unoccupied Cooling Setpoint Unoccupied Cooling Setpoint
Unoccupied Heating Setpoint Unoccupied Heating Setpoint
Zone/Space Temperature Zone/Space Temperature