COBP system setup procedures - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
The Verasys zone controllers come with predefined parameters and are easy to configure when they communicate to the zone coordinator. However, you must configure the system to ensure proper operation and control of the equipment connected to the devices. This section instructs you how to set up the zone coordinator for a COBP system.