VAV controller zone setup procedures - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
The Verasys zone controllers come with predefined parameters and are easy to configure when they communicate to the zone coordinator. However, you need to configure temperature control and flow control to ensure proper operation and control of the equipment connected to the devices. This section instructs you on how to set up the zone controllers for temperature and flow control. Refer to Verasys ZEC510 VAV Controllers Installation Guide Part No. 24-10143-01485.