Using the backup feature, you can save all the settings for the device into a file. You can back up an individual device or all of the devices simultaneously. Backup is supported on all SMART Equipment controllers. The following table shows controller backup version requirements.
Controller | Version |
---|---|
Verasys Application Controllers | All versions |
TEC3000 Thermostats | 3.0.0.0128 and newer, wired 2.0.0.1007 and newer, wireless |
Simplicity Smart Equipment Rooftop | 3.3.1.186 and newer |
VZC/ZEC/BYP | All versions Note: The ZEC310 and ZEC510 are backed up as part of
the VZC100 backup. Restoration of the VZC100 backup restores the information to the
VZC100 in addition to the ZECs and BYP.
|
To back up a device, complete the following steps:
- Navigate to the Settings tab, and click the Backup tab.
- From the Select device for backup drop-down list, select the device that you want to backup.
- Click Backup All. Note: During a backup procedure, a progress bar appears for all the devices included in the backup. Successful backups appear with a completed progress bar at 100% and a Close button. When the backup fails, an error message appears and your backup does not appear in the list.
- When the backup completes, close the progress bar. The system updates the time stamp and stores the file. You can also download individual files with the download icon. The files download to the location setup in your Internet browser. This is usually your downloads folder. The backups are usually saved locally to the PC according to your browser settings. If you use Google Chrome, the files are saved to C:\Users\<username>\Downloads. To remove the file, click the trash can icon.
Use the check boxes on the left to select any, or all of the files to download one backup file for all the selected controllers. The file transfers to your download folder on Microsoft® Windows® operating system. You can also download individual files with the download icon. To remove a file, click the trash can icon. Refer to the follwing video link https://docs.jci.com/bas/verasys-backup-restore.