Configuring a one-condition interlock - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
Verasys System User Guide
- Brand
- Verasys
- Product name
- Verasys System
- Document type
- User Guide
- Document number
- LIT-12012371
- Version
- 4.2
- Revision date
- 2023-06-15
- Product status
- Active
- Language
- English
Procedure
-
If you want, provide a name and description for your interlock.
-
On the Interlock
Condition area, from the Device drop-down list
select the device that you want to associate with
the interlock to show all the points you can
assign between the device and the interlock.
-
From the Points drop-down list, select the Point you want to
associate with the interlock. This action makes the point part of the Interlock
logic.
-
From the Operator drop-down list, select the operator for the point.
-
Enter the value.
-
Enter the Differential +/-
variance. Differential will only be available if an analog data point is selected.
-
Under Input Conditions, select One Condition.
-
In the Interlock Action area, select the device and point on which you
want to perform the interlock action. You can configure an action when the interlock
is true or false.
-
Click Save to enable the interlock.