Changing the name of a facility - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
You can change the name of a facility to the name of the building or site it controls. This name appears in the place of Facility in the SBH menu structure. To change the name, complete the following steps:

  1. Navigate to Settings and select Alarm Notifications.
  2. Navigate to the Site Name field and change the name.
  3. Click Save.