HVAC view - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
The Facility view for HVAC has four or five columns, depending on what controllers are connected to the network. The name of the space appears in the first column, beside the + symbol. The space names come from the device that controls a particular space.

The second column contains information about the space temperature. The color of the text depends on the space status.

The third column displays the space status. The Status column displays as one of the following parameters:

  • HEATING
  • COOLING
  • SATISFIED
  • FAULT
  • UNAVAILABLE
  • SYSTEM OFF

The fourth column displays the space occupancy status, either Occupied or Unoccupied.

The optional fifth column appears on devices with energy indicator setbacks. An extra option to reset the setpoints back to energy efficient default values appears if the controllers on the network provides it.

If you select the + symbol, the Facility view expands to a simplified graphical user interface. The current temperature and status of the space change colors depending on the status of the facility. The setpoints that the space controls appear below the circle. You can use the up and down arrows to adjust the actual setpoint. You can use the unit enable button to shut down or enable the unit. You can use the system mode drop-down menu to set the system mode to cooling, heating, or automatic.

In the bottom right corner, a link to the equipment associated to the space appears. Select the link to gain access to the Equipment details page. With the appropriate access rights, you can click the Equipment shortcut to adjust other parameters. In addition to the equipment link, there are icons that directly take you to the alarms, schedules, or trends of that device.

Note: Access rights are granted to you when you sign in using your password.