Configuring a two-condition interlock - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
Verasys System User Guide
- Brand
- Verasys
- Product name
- Verasys System
- Document type
- User Guide
- Document number
- LIT-12012371
- Version
- 4.2
- Revision date
- 2023-06-15
- Product status
- Active
- Language
- English
Procedure
-
If you want, provide a name and description for your interlock.
-
On the Interlock Condition area, from the
Device dropdown list select the device that you want
to associate with the interlock to show all the points you can assign between
the device and the interlock.
-
From the Points dropdown list, select the
Point you want to associate with the interlock. This
action makes the point part of the interlock logic.
-
From the Operator dropdown list, select the operator for
the point.
-
Enter the value.
-
Enter the Differential +/- variance.
-
Under Input Conditions, select Two Conditions
(AND) or Two Conditions (OR).
-
Follow a similar process to steps 3-5 above for first input condition .
-
In the Interlock Action section, select the device and
point which you want to perform the interlock action. You can configure an
action when the interlock is true or flase.
-
Click Save to enable the interlock.