Use the restore feature to restore the backed-up controller setting to the selected device. You can restore an individual device or all of the devices. Restore is supported on Verasys Smart Equipment controllers. See Table 1 for supported controller versions.
To perform a restore procedure, complete the following steps:
- Navigate to the Settings > Restore.
- Under Restore Devices, select the device from the drop-down list.
- Choose whether to restore from a file or the SBH.
- If you choose to restore from a file, click Choose File and select the controller backup file that you want to restore, click Open. When the file name appears in the choose file display box, click Upload. If the controller is within the download file, the Restore Settings information appears.
- On the Timestamp Column of the file displayed, identify the file you want and click the Radio Button on the far right to select the file. Click Restore. The devices reboot after the restore procedures.
- To select another backup file, navigate to Settings >
Restore. Note: Devices reboot after restore procedures. If the device you selected is not in the download file, a circular icon appears. You can switch to the Backup tab and see which devices have associated backup files. When you restore from a file, the data overwrites the data on the SBH.
- To restore a backup from the files on the SBH, select the From SBH button and the device that you want to restore. If the device has a backup file on the SBH, the file appears and you can load it. Follow step 5 above if no file appears, return to the Backup tab and check that the device has an associated backup file.