Testing the unit - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
Verasys System User Guide
- Brand
- Verasys
- Product name
- Verasys System
- Document type
- User Guide
- Document number
- LIT-12012371
- Version
- 4.2
- Revision date
- 2023-06-15
- Product status
- Active
- Language
- English
- Navigate to the VEC Commissioning page to test the unit.
- Before you turn on the fan, block zones open or ensure the bypass damper is
operational.
- Set the Start Commission parameter to
Trigger.
- Turn on the fan.
- Turn on the heating stages and make sure the SAT increases.
- Turn on the cooling stages and make sure the SAT decreases.
- To finish testing the unit, set the Start Commission parameter back to
Normal.