The second set of options for this feature are for a BACnet IP Broadcast Management Device (BBMD). The BBMD enables an SBH on one subnet to communicate with a supervisory device on another subnet.
To set up the router feature for the BBMD, complete the following steps on the SBH and the supervisor:
- On the SBH, configure the following for each BBMD:
- IP Address – The IP address of the supervisor with which the BBMD communicates.
- UDP Port –UDP Port of the supervisor with which the BBMD communicates. It is different from the UDP port of the SBH itself.
- IP Broadcast Mask – Needs to match on both the SBH and the supervisor.