Setting exceptions - Verasys - LIT-12012371 - LC-SBH200-0 - Building automation software - Verasys System - 4.2
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
About this task

As part of the schedule functionality, you can set exceptions such as holidays, or any other exceptions to a normal weekly schedule. To set an exception, complete the following steps:

Procedure

  1. Click Schedules.
  2. Click the Modify icon of the schedule you want to add an exception to.
  3. Click Exceptions.
  4. Click +Add Exception. The maximum number of exception schedules allowed is 20.
  5. Select the required dates for the exception. As you select the dates, they appear in the Selected Dates field.
  6. Select the time and the value for the exception. If you want to add more times and values, click +Add New Event to add a new time and value field.
  7. Click OK.
    Important: When you save the new exceptions, the schedule is not yet saved. Continue with the next step to save the schedule.
  8. Click Save to save the schedule with the new exceptions.