Occupancy lighting switch (optional) - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document revision
D
Revision date
2019-07-01
Product status
Discontinued
Part number
24-10143-1248
  • You can add an occupancy lighting switch to the box to temporarily set the controller to standby mode it does not detect occupancy. When the box detects occupancy, the zone switches back to occupied mode.
  • Standby mode uses standby temperature setpoints that are slightly higher or lower than the occupied cooling or heating setpoints, respectively.