Supply power terminal block - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document revision
D
Revision date
2019-07-01
Product status
Discontinued
Part number
24-10143-1248

The 24 VAC supply power terminal block is a gray, removable, 2-terminal plug that fits into a board-mounted jack on the upper left of the ZEC/BYP controller. Wire the 24 VAC supply power wires from the transformer to the terminal plug as shown on the following figure.

Note: The supply power wire colors may be different on transformers from other manufacturers. Refer to the transformer manufacturer's instructions and the project installation drawings for wiring details.
Figure 1. VAC Supply power terminal block wiring

Table 1. VAC Supply power terminal block wiring
Calllout Description

1

Supply power terminal block jack

2

Supply power terminal block plug

3

Wires from Johnson Controls 90 VAC to 24 VAC, Class 2, power transformer
Important: The 24 VAC power should not be shared with other network devices. Sharing power with other network devices may cause noise, interference, and ground loop problems. You may damage the controller by sharing power with other devices.