Occupancy Sensor - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document type
Installation Guide
Document revision
D
Revision date
01/07/2019
Part number
24-10143-1248

All zone controllers support an occupancy sensor. The occupancy sensor enables the controller to switch from occupied mode to standby mode. This occurs in normal occupied mode during a set time period, when local activity is absent. When in standby mode, the zone controller uses standby temperature setpoints that are higher and lower than the occupied cooling and occupied heating temperature setpoints. These standby setpoints save energy by reducing the demand for heating and cooling in an unoccupied zone. For Zone Dampers, the sensor uses unoccupied flow setpoints in addition to standby temperature setpoints. You can enable the occupancy sensor in the Zone Setup screen of the System Manager or Zone Coordinator. You can set occupancy sensitivity and time delay until standby locally at the sensor. Refer to the Verasys System User’s Guide (LIT-12012370) for more information.