I/O wiring - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document revision
D
Revision date
2019-07-01
Product status
Discontinued
Part number
24-10143-1248

It is important that the ZEC/BYP controller is wired properly. If the ZEC/BYP controller is wired incorrectly, communication problems can occur. These problems include devices going online and offline, or devices not coming online at all.