Wiring - Verasys - LC-BYP200-0 - LC-ZEC310-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document type
Installation Guide
Document revision
D
Revision date
01/07/2019
Part number
24-10143-1248
CAUTION
  • Risk of Electric Shock
  • Disconnect the power supply before making electrical connections to avoid electric shock.
ATTENTION
  • Risque de décharge électrique
  • Débrancher l'alimentation avant de réaliser tout raccordement électrique afin d'éviter tout risque de décharge électrique.
Important: Make all wiring connections in accordance with the National Electrical Code and local regulations. Use proper electrostatic discharge (ESD) precautions during installation and servicing to avoid damaging the electronic circuits of the controller.
Important: Do not exceed the controller electrical ratings. Exceeding controller electrical ratings can result in permanent damage to the controller and void any warranty.
Important: Do not connect supply power to the controller before finishing wiring and checking all wiring connections. Short circuits or improperly connected wires can result in damage to the controller and void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with local, national, and regional regulations.
Important: Maintain proper polarity and voltage or current ratings. Improper polarity or exceeding the voltage or current ratings voids the warranty.