- You can proportionally reset the minimum damper positions based on an air quality setpoint when you wire the zone CO2 sensors to the controller to detect the air quality in the zone.
- The reset of the damper minimum positions do not exceed the maximum value that you set. When the CO2 sensor is not connected, the controller uses the cooling minimum position and the heating minimum position.
Figure 1. BYP200 wiring diagram

|
Callout |
Description |
Object name |
|---|---|---|
|
1 |
Bypass damper output |
BYPD2-O |
|
2 |
Manual override |
n/a |
|
3 |
Discharge air static pressure |
DA-P |
|
4 |
To next device |
n/a |
|
5 |
From last device |
n/a |
|
6 |
24 V HOT |
n/a |
|
7 |
24 V COM |
n/a |
|
8 |
24 V HOT |
n/a |