Duct static pressure probe requirement - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document revision
D
Revision date
2019-07-01
Product status
Discontinued
Part number
24-10143-1248

The Bypass Damper requires the use of a duct static pressure probe (FTG618A-600R) and 6.4 mm (1/4 in.) I.D. user-supplied tubing. The tubing must connect to the probe and link the H1 (+) port of the pressure sensor, located on the Bypass Damper controller.