PCX Expansion Input/Output Module - Facility Explorer - LIT-12011657 - Accessory - Field Device - Handheld VAV Balancing Sensor/Tool - FX-PCV19 Programmable VAV Box Controller - FX-PCX27 Expansion Input/Output Module - FX-PCV18 Programmable VAV Box Controller - FX-PCG26 General Purpose Programmable Controller - FX-PCX47 Expansion Input/Output Module - FX-PCA36 Advanced Application Programmable Controller - FX-PCG16 General Purpose Programmable Controller - FX-PCA49 Advanced Application Programmable Controller - FX-PCV16 Programmable VAV Box Controller - FX-PCX17 Expansion Input/Output Module - FX-PCA26 Advanced Application Programmable Controller - FX-PCX37 Expansion Input/Output Module

FX-PC Series Programmable Controllers and Related Products Product Bulletin

Product
Variable Air Volume > Tools > Handheld VAV Balancing Sensor/Tool
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV19 Programmable VAV Box Controller
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV18 Programmable VAV Box Controller
Controls > Programmable Controls > FX-PCG26 General Purpose Programmable Controller
Controls > Input/Output Controls > FX-PCX47 Expansion Input/Output Module
Controls > Programmable Controls > FX-PCA36 Advanced Application Programmable Controller
Controls > Programmable Controls > FX-PCG16 General Purpose Programmable Controller
Controls > Programmable Controls > FX-PCA49 Advanced Application Programmable Controller
Variable Air Volume > Variable Air Volume Box Controls > FX-PCV16 Programmable VAV Box Controller
Controls > Input/Output Controls > FX-PCX17 Expansion Input/Output Module
Controls > Programmable Controls > FX-PCA26 Advanced Application Programmable Controller
Controls > Input/Output Controls > FX-PCX37 Expansion Input/Output Module
Document type
Product Bulletin
Document number
LIT-12011657
Revision date
2022-07-19
Product status
Active

The PCXs are expansion I/O modules with integral RS-485 MS/TP communications.

Note: At Controller Configuration Tool (CCT) Release 10.1 and later, the PCGs, PCAs, and PCVs can communicate by using either the BACnet or the N2 field bus networking protocol. The operation of the PCX is not affected by the selection of the BACnet or the N2 protocol in the host controller.

PCXs can serve in one of two capacities, depending on where they are installed in the control system. When installed on the Sensor Actuator (SA) Bus of equipment controllers, the PCXs expand the I/O interfaces of the controllers. When installed on the Field Controller (FC) Bus, PCXs can be used as I/O point multiplexors to support monitoring and control from a supervisory controller. The point multiplexor can also be useful for sharing points between other PC controllers on the FC Bus using peer-to-peer connectivity.

A full range of equipment controllers combined with the PCX models can be applied to a wide variety of building applications ranging from simple fan coil or heat pump control to advanced central plant management.