Procedure
To view input and output equipment data at a site, complete the following steps:
-
Select a site. For more information, see Selecting one site or multiple sites.
The tabs for the equipment types at the site appear on the dashboard.
-
Click the I/O tab.
The I/O tab displays a list of all of the input and output controllers at the site, and for a selected controller, a table and a chart for each input and output type. The table lists data about all the connected ports of the given input or output type, and the chart displays historical data of one selected port. The I/O tab also includes a summary of the alarms on the selected controller.
- Select the controller you want to view from the Select IOM Controller drop-down list.
- To change to a larger view of a table or chart and then back to the original size, click the Zoom icon in the upper right corner of the table or chart.
-
To override binary outputs in a controller that uses binary
outputs, complete the following steps:
- In the Binary output table, click inside the Override column for the binary output you want to override.
- In the Binary Output Override window, select a value in the Override To drop-down list, and click Command.
- To view the history of input and output values in a chart, see the trend area for each input and output type. Select the input or output point from the drop-down menu. For more information about customizing the chart, see Customizing charts in Verasys Enterprise.
- To view the active alarms on the IOM controller, see the Alarm summary area. To download the alarm list in CSV format, click the Download icon. To view the alarm history for the controller in a separate pop-up window, click the History icon. In the Alarm History window, click the Download icon to download the alarm history list in CSV format.