When you select a site, the Verasys Enterprise dashboard shows data about that site and tabs appear above the connected sites widget.
You can use the tabs to access specific information and functions for different types of equipment at the site. If a type of equipment is not present at the site, the corresponding tab does not appear. The following figure shows a part of a site dashboard with tabs.
Figure 1. Verasys Enterprise site dashboard with tabs
The following table lists the available tabs and their functionality.
Tab name | Function |
---|---|
Overview | Display the site dashboard main page. |
HVAC | View data about HVAC equipment at the site and change setpoints. |
Lighting | View and control lighting equipment at the site. |
I/O | View data about input and output equipment at the site. |
Energy | View data about voltage, current, energy consumption, and energy demand at the site. |
Refrigeration | View data about refrigeration equipment at the site and change setpoints. |
Schedule | View and create schedules for the equipment at the site. |
Misc. | View data about third-party BACnet equipment at the site. |