Procedure
To create a new schedule on one or more controllers on one or more sites, complete the following steps:
- Select one site or multiple sites. For more information, see Selecting one site or multiple sites.
- From the nine-dot menu, select Schedules.
-
To create a schedule for analog inputs, click the Analog
Schedule tab. To create a schedule for multistate inputs, click
the Multistate Schedule tab.
Note: If the controller selection panel displays No Data Available, no controllers at any selected site support schedules for the given input type.
- Select the schedule type from the Schedule Type drop-down list.
- In the controller selection panel, expand the sites or search for the controller or controllers that you want to create the schedule for.
- To add weekly events or exceptions to the schedule, click the Weekly Schedule or Exception Schedule tab and click Add Event.
- In the Add Event window, set the event times and click New Event. When you finish, click Save.
- To switch to the calendar view for the weekly schedule or exception schedule, click the Calendar icon. To switch back to table view, click the Table icon.
- To save a weekly schedule or exception schedule, click Save Weekly Template or Save Exception Template. In the Save Template window, enter a name for the template and click Save.
- To import a weekly schedule or exception schedule, click Import Weekly Template or Import Exception Template. In the Import Template window, select a template from the drop-down menu and click Import.