Procedure
To view the details of individual lighting controllers and zones on one site and to control the lighting, complete the following steps:
-
Select a site. For more information, see Selecting one site or multiple sites.
The tabs for the equipment types at the site appear on the dashboard.
-
Click the Lighting
tab.
The Lighting tab displays a list of all of the lighting controllers and the related lighting zones at the site.
-
To change the lighting for a zone, click inside the Master Override column of the zone. The
Override window appears. Choose from
the following options:
- To issue a master override command, select Auto, On, or Off from the Master Override drop-down list.
- To issue a temporary override command, click Temporary Override. To release a temporary override command before the override duration finishes, click Release Temporary Override.
Verasys Enterprise sends the override command to the controller and displays a notification about the result.
- To change the override duration, click inside the Override Duration column for the zone. The Override Duration window appears. Type in the duration value or use the arrow buttons to change the value, and click Command.
- To view the history of lighting commands in a chart, see the Raw Samples - Zone Command area. Select the zone from the drop-down menu. For more information about customizing the chart, see Customizing charts in Verasys Enterprise.