Procedure
To view energy data, complete the following steps:
-
Select a site. For more information, see Selecting one site or multiple sites.
The tabs for the equipment types at the site appear on the dashboard.
-
Click the Energy
tab.
The Energy tab displays a list of all of the controllers at the site that have energy meters. You can view data about voltage, current, energy consumption, and energy demand for a controller that you select.
- Select the controller you want to view from the Select Controller drop-down menu.
- To change to a larger view of a table or chart and then back to the original size, click the Zoom icon in the upper right corner of the table or chart.
- To view the history of voltage and current values in a chart, see the Voltage trend and the Current trend area. Select the energy meter from the drop-down menu. For more information about customizing the charts, see Customizing charts in Verasys Enterprise.
- To view the history of energy consumption and the energy demand minimum, maximum, and average values, see the Consumption and the Demand areas. Select the energy meter from the drop-down menu. For more information about customizing the charts, see Customizing charts in Verasys Enterprise.