Procedure
To view and edit existing schedules at a site, complete the following steps:
- Select one site or multiple sites. For more information, see Selecting one site or multiple sites.
- From the nine-dot menu, select Schedules to see a list of the existing schedules. As an alternative, if you select one site, click the Schedule tab.
- In the schedule list, click the schedule you want to edit. The calendar view opens.
- To edit or delete an event, double-click the event in the calendar and in the pop-up window, click Edit Event. In the Edit Event window, modify the event parameters and click Save. To delete the event, click Delete.
- To add a new event, double-click an empty time slot in the calendar. In the New Event window, set the event parameters and click Save.