Procedure
To view the details of individual HVAC controllers on one site and to change setpoints and the controller graphic, complete the following steps:
-
Select a site. For more information, see Selecting one site or multiple sites.
The tabs for the equipment types at the site appear on the dashboard.
-
Click the HVAC tab.
The HVAC tab displays a list of all of the heating, ventilation, and air conditioning controllers at the site.
-
Click a row in the list.
The HVAC Detail page opens and displays a graphic, detailed information, and charts about the controller.
-
To change a setpoint in the Set
points area, type the new value or click the arrow buttons to
change the value, and click Apply
Setpoint.
Verasys Enterprise sends your setpoint change command to the controller and displays a notification with the result.
- To add or change the graphic for the controller, click Choose file, select the graphic file, and click Upload.
- To view trend data for the controller, see the Trend chart area. To select a maximum of four trend points to display on the chart, click Select Point. For more information about customizing the chart, see Customizing charts in Verasys Enterprise.
-
To view status trend data for the controller, see the
Status trend chart area. For more
information about customizing the chart, see Customizing charts in Verasys Enterprise.
Note: This chart appears if the controller contains status trend points.
- To view the active alarms on the controller, see the Alarm summary area. To download the alarm list in CSV format, click the Download icon. To view the alarm history for the controller, click the History icon. In the Alarm History window, click the Download icon to download the alarm history list in CSV format.
- To view data that can help diagnose faults, see the Fault Detection Diagnostics area for the controllers that support this feature. To view the present value of all points in a table format, click the Table icon. To view the data as a chart, click the Chart icon, and select the point to display on the chart in the drop-down menu. For more information about customizing the chart, see Customizing charts in Verasys Enterprise.