Procedure
You can use the batch setpoint change feature to change the
setpoints of multiple HVAC controllers at different sites at the same time. To
perform batch setpoint changes, complete the following steps:
-
Select multiple sites. For more information, see Selecting one site or multiple sites.
-
In the nine-dot menu, select Setpoints.
The HVAC Setpoints page opens.
-
In the left-hand pane of the HVAC
Setpoints page, expand the selected sites and the controllers.
Select the checkbox of the controllers whose setpoints you want to change.
When you select the controllers, the individual and common setpoints of the
controllers appear in the main content area.
-
In the main content area of the HVAC
Setpoints page, enter a value for the setpoints that you want to
change, or change the value with the arrow buttons, and click Apply Batch Setpoints.
A confirmation window opens that lists all your setpoint change commands to
the controllers. If you want to proceed with the setpoint changes, click
Yes.
After you confirm the changes, Verasys Enterprise sends the setpoint change
commands, and displays the Result
Summary window that lists the result of each setpoint change
command.