USB Port - Verasys - LC-MAP1860-1SL - Supervisory controller - Verasys Smart Building Hub

Verasys Smart Building Hub (SBH) Installation Guide LC-MAP1860-1SL

Product
Building Automation Systems > Building Automation Systems > Verasys Smart Building Hub
Document revision
A
Revision date
2021-03-26
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10737-00180
Note: USB port functionality is not available in this software release.

The USB port on the Smart Building Hub is a 5-pin, Micro-B peripheral serial port which conforms to the USB 2.0 standard. The Smart Building Hub USB port is for connecting to a computer for commissioning, downloading, and retrieving data. When the Smart Building Hub is connected and powered from the USB port, FC bus functions are not available.

Note: The USB connection on the Smart Building Hub is not designed for constant use. The USB port should be used only when needed.
Table 1. USB Port Pin Designations
Pin Number (Both Ends of Cable) Signal Name
1 +5 VDC
2 Data -
3 Data +
4 No Connection
5 Ground