Special Tools Needed - Verasys - LC-MAP1860-1SL - Supervisory controller - Verasys Smart Building Hub

Verasys Smart Building Hub (SBH) Installation Guide LC-MAP1860-1SL

Product
Building Automation Systems > Building Automation Systems > Verasys Smart Building Hub
Document type
Installation Guide
Document revision
A
Revision date
26/03/2021
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10737-00180

To use the Smart Building Hub, you need a mobile device (tablet or Smart phone) or computer (laptop or desktop) that supports Wi-Fi.

If the unit is mounted to a vertical surface without a DIN rail, you need screws to mount the unit. The specific screw types depend upon the surface to which the unit is mounted. The screw holes on the Smart Building Hub can accommodate M3.5 and #6 screws.

Use of the mounting bracket locking screw requires a T15 Torx driver.