Location Considerations - Verasys - LC-MAP1860-1SL - Supervisory controller - Verasys Smart Building Hub

Verasys Smart Building Hub (SBH) Installation Guide LC-MAP1860-1SL

Product
Building Automation Systems > Building Automation Systems > Verasys Smart Building Hub
Document revision
A
Revision date
2021-03-26
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10737-00180

Observe the following guidelines when mounting a Smart Building Hub:

  • Mount the Smart Building Hub in areas free of corrosive vapors and observe the environmental limitations listed in the Technical Specifications section of this document.
  • Objects (including ductwork, cabinets, doors, and glass) can impede the wireless signal. Minimize the number of objects between the connected computer or mobile device computer and the Smart Building Hub. Use line of sight, if possible.
  • Metal objects (such as cabinet doors, enclosures, and pipes) and concrete objects (such as pillars, walls, and ceilings) may limit Wi-Fi service. To accommodate potential structural obstacles on site, the Smart Building Hub can be mounted flush against the wall or perpendicular to it.
  • The Smart Building Hub is not rated for outdoor mounting.