- power
- fault
- FC bus communication
- Ethernet communication
- Wi-Fi strength
See Table 1 for a comprehensive list of Smart Building Hub LED functional information.
| LED Name |
Color | Normal | Descriptions/Other Conditions |
|---|---|---|---|
| Power | Green | On Steady(no flashing) |
Off = No power
On Steady = Power supplied by primary voltage |
| Fault | Red | Off |
Off = No
faults/normal operation On Steady = Missing hardware, missing software, operating system has not yet initialized, or reset is in progress. Slow Flicker (1 blink per second) = Software upgrade in progress Medium Flicker (2 blinks per second) = Startup sequence Fast Flicker (5 blinks per second) = Fault |
| FC Bus | Green | Flicker |
Off = Receiving
data On Steady = Transmitting data Flicker = Data transmission |
| Ethernet | Green | On Steady |
Off = Communication
not established On Steady = Communication established Flicker = Data transmission |
| Wi-Fi | Yellow | On Steady |
Off = No Wi-Fi
signal Wi-Fi strength is indicated by the number of LEDs that are lit, with one lit LED indicating weak wireless signal strength (between 1%and 49%) and three lit LEDs indicating excellent wireless signal strength (at least 75%). |