LED Test Sequence at Startup - Verasys - LC-MAP1860-1SL - Supervisory controller - Verasys Smart Building Hub

Verasys Smart Building Hub (SBH) Installation Guide LC-MAP1860-1SL

Product
Building Automation Systems > Building Automation Systems > Verasys Smart Building Hub
Document type
Installation Guide
Document revision
A
Revision date
26/03/2021
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10737-00180
During startup, the Smart Building Hub automatically initiates a self-test to verify proper operation of the unit. Immediately after connecting supply power, the following LED lighting sequence occurs:
  • The power LED turns on, and stays lit.
  • The Fault LED indicator flashes for approximately 40 seconds, then turns off when the Smart Building Hub is fully functional.
  • The Wi-Fi LEDs light up in succession (scanning), indicating that the Smart Building Hub is waiting for a device to join its Wi-Fi network.