Configuring the binary outputs - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

Binary outputs 1 and 2 connect to the two stages of the Electric Unit Heater. Binary output 3 connects to the fan, and binary output 4 connects to the damper.

Configuring binary output 4 for EFD-C

To configure binary output 4, complete the following steps:

  1. On the SBH, navigate to Details > Outputs > Binary Output 4.
  2. Set the following parameters:
    1. Present to Present
    2. Description to EFD-C

Configuring binary output 3 for EF-C

To configure binary output 3, complete the following steps:

  1. On the SBH, navigate to Details > Outputs > Binary Output 3.
  2. Set the following parameters:
    1. Present to Present
    2. Description to EF-C

Configuring binary output 1 and 2 for the Electric Unit Heater

To configure binary outputs 1 and 2, complete the following steps:

  1. On the SBH, navigate to Details > Outputs > Binary Output 1.
  2. Set the following parameters:
    1. Present to Present
    2. Description to Heater stage 1
  3. Navigate to Details > Outputs > Binary Output 2.
  4. Set the following parameters:
    1. Present to Present
    2. Description to Heater stage 2