Configuring the binary inputs - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

Binary input 2 supplies the damper status, and binary input 1 supplies the fan status.

Configuring binary input 2 for EFD-S monitoring

To configure binary input 2, complete the following steps:

  1. On the SBH, navigate to Details > Inputs > Binary Input 2.
  2. Set the following parameters:
    1. States Text to Off/On
    2. Description to EFD-S

Configuring binary input 1 for EF-S monitoring

To configure the binary input 1, complete the following steps:

  1. On the SBH, navigate to Details > Inputs > Binary Input 1
  2. Set the following parameters:
    1. States Text to Off/On
    2. Description to EF-S