Configuring network shared inputs - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English
Through the data share feature on the SBH and MAP, you can configure one temperature-based process variable and one temperature-based PID setpoint.
Note: Any control loops configured to use either network shared process variable or setpoint share the same value. It is not possible to configure a separate process variable or setpoint for each individual control loop.