Configuring binary inputs - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

Configure binary inputs in the Details > Inputs menu. Define the texts for the different states, add a description, and define alarm information for each connected binary input.

Trend data is available automatically for each connected binary input.