Introduction - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

The Verasys® sideloop controller application is part of the Verasys application library.

To download the application, log in to verasyscontrols.com and access the application library in the Product Information & Support > Device Updates section. Download the application package file and install it on the Verasys Application Controller (VAC), LC-VAC1000-0. See Updating the VAC for more information.

This document describes the application, wiring, and characteristics of the controller. The parameters for this controller are adjustable in the field, but the application is fixed.

If you have further questions about the application, contact Verasys support.