Setting the VAC address using the SBH - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

About this task

To set the VAC address using the SBH, perform the following steps:

Procedure

  1. In the SBH, navigate to the VAC controller.
  2. Navigate to the Controller > Network menu of the VAC controller.
    Note: The default address is 4. If another controller uses this address, disconnect the other address 4 controller from the trunk temporarily while you configure the controller, or use the procedure in Setting the VAC address using the local display.
  3. Click the Up and Down arrows to select the address, or enter the address directly.
  4. Click Save.