Updating the VAC - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

About this task

To update the VAC, perform the following steps:

Procedure

  1. Navigate to verasyscontrols.com, and log in with your credentials.
  2. Navigate to Product Information & Support > Device Updates.
  3. Download the package file for the Verasys Sideloop application to the root folder of a USB 2.0 drive. The package file name is the following: VAC1000 - Verasys Sideloop Controller_xxxx.pkg.
    Note: Ensure that the USB drive is formatted as FAT or FAT32.
  4. Insert the USB drive into the USB port on the LC-VAC1000-0 controller.
  5. If the download does not start immediately, then in the controller’s local display, select the Update and Load Firmware option, then choose the package file on the USB drive, and press Enter.
  6. When the application update finishes, use the Verasys Smart Building Hub (SBH) or the local display to configure the controller.