Configuring binary outputs - Verasys - LIT-12013364 - LC-VAC1000-0 - Smart equipment controller - VAC1000 - 4.2

Verasys Sideloop Controller Application Note

Brand
Verasys
Product name
VAC1000
Document type
Application Note
Document number
LIT-12013364
Version
4.2
Revision date
2021-07-16
Product status
Active
Language
English

Configure binary outputs in the Details > Ouputs menu. Set the output presence, add a description, and define override and polarity settings for each connected binary output.

Trend data is available automatically for each connected binary output.