To change the same attribute values of many objects, use the WritePropertyMultiple
method. This method accepts an optional write priority.
Library method name |
WritePropertyMultiple
|
---|---|
Description | Write multiple properties to multiple objects. |
Method signature |
void WritePropertyMultiple(IEnumerable<Guid> ids,Dictionary<string, object> attributeValues
|
Method input parameters |
|
Return value | None |