Overview - Metasys - LIT-12013522 - Software Application - Basic Services client library for .NET (and COM) - Metasys API - 4.2

Metasys REST Client for .NET and COM Developer Guide

Product name
Basic Services client library for .NET (and COM)
Metasys API
Document type
API Reference Guide
Document number
LIT-12013522
Version
4.2
Revision date
2021-04-07

The DLL contains the library that uses the .NET client to access the Web API to access the Metasys objects.

For an overview of how the command line application, Microsoft Excel®, and weather forecast application query the Metasys system using the Metasys library, see the following diagram.

Figure 1. Applications query Metasys System