Installing the Metasys client library - Metasys - LIT-12013522 - Software Application - Basic Services client library for .NET - Metasys API - 4.2

Metasys REST Client for .NET and COM Developer Guide

Product
Building Automation Systems > API > Metasys API
Document type
API Developer Guide
Document number
LIT-12013522
Version
4.2
Revision date
2021-04-07

Install NuGet packages using Microsoft package consumption workflow. For more information, see https://docs.microsoft.com/en-us/nuget/consume-packages/overview-and-workflow

If you want to use the DLL in a .NET application, include the following .NET C# code in the target source files;
using JohnsonControls.Metasys.BasicServices;

To install the DLL, consume the package using one of the following options:

  • Consuming the package using the PackageReference method.
    • Add the following code to the project's .csproj file:
      <ItemGroup>
          <PackageReference Include="JohnsonControls.Metasys.BasicServices" Version="<target version>" />
      </ItemGroup>
      
  • Consuming the package using the command line interface
    1. Open a command line and navigate to your project's main directory.
    2. Execute the following command:
      nuget install JohnsonControls.Metasys.BasicServices -OutputDirectory packages
    3. Update all packages with command:
      nuget restore

    If you want an alternative to using the command line, use Microsoft Visual Studio. The following image shows a successful package install.

Figure 1. Package installation using Microsoft Visual Studio®