Use the following menu to test the client library
methods:1) TryLogin, Refresh
2) GetObjectIdentifier
3) ReadProperty
4) ReadPropertyMultiple
5) WriteProperty
6) WritePropertyMultiple
7) GetCommands
8) SendCommand
9) GetNetworkDeviceTypes, GetNetworkDevices
10) GetObjects
11) Localize
12) GetSpaces
13) GetSpaceTypes
14) GetEquipment
15) GetSpaceEquipment, GetSpaceChildren
16) GetEquipmentPoints
17) GetAlarms
18) GetSingleAlarm, GetAlarmsForAnObject, GetAlarmsForNetworkDevice
19) GetAlarmAnnotations
20) GetTrendedAttributes, GetSamples
21) GetAudits
22) GetSingleAudit, GetAuditsForAnObject
23) GetAuditAnnotations
24) DiscardAudit
25) ChangeApiVersion
26) ChangeHostname
27) AddAuditAnnotation
28) AddAuditAnnotationMultiple
29) DiscardAuditMultiple
30) GetServerTime
99) Exit
Select an option: