Open Weather Map API application - Metasys - LIT-12013522 - Software Application - Metasys API - Basic Services client library for .NET - 4.2

Metasys REST Client for .NET and COM Developer Guide

Product
Building Automation Systems > API > Metasys API
Document type
API Developer Guide
Document number
LIT-12013522
Version
4.2
Revision date
2021-04-07

Open Weather Map services provide three-hour forecasts for temperature, humidity, snow, and rain. If you have to configure a Metasys system according to weather precipitations, you could use the Metasys API to integrate with Open Weather Map API application. In this example, you must provide the latitude and longitude coordinates of the site as inputs to get a response of separated points for each type of precipitation.

Figure 1. Metasys UI for weather forecast details