The following tables provide examples of valid and invalid string references and a description explaining the format.
The Application Data Server (ADS) and the Network Automated Engine (NAE) are used is the following examples.
Reference | Description |
---|---|
ads35:ads35 | Refers to a device with the computer name ads35 that is a child of the Site Director with the same name. |
ads35:ads35/$site | Refers to a site object that is on the Site Director with the computer name ads35. |
ads35:ads35/Programming | Refers to an object named programming on a device with the computer name ads35 that is a child of the Site Director with a computer name ads35. |
ads35:nae3 | Refers to a device with the computer name nae3 that is a child of the Site Director with the computer name ads35. |
ads35:nae35/Programming.AV1 | Refers to an object named AV1 under an object named programming on a device with the computer name nae35 that is the child of the Site Director with a computer name ads35. |
Reference | Description |
---|---|
ads35:nae23/$site | Refers to a site object on a child device. A child device cannot have a site object. |
ads35/Programming | The portion before the forward slash must comply with this format:
|
ads35 | The reference must comply with this format:
|